Skip to main content
MJo.3
Associate II
July 10, 2023
Solved

[stm32mp157D] Two board have different number of cpu when I use lscpu

  • July 10, 2023
  • 1 reply
  • 1911 views

Hi,
I bought two same board and use one to test.
After upgrade stlinux on this testing board, the cpu it can recognize is only one when the other one can recognize it two.
could you give me a guide to fix it and why this happened?

Thanks.

This topic has been closed for replies.
Best answer by Olivier GALLIEN

Hi @MJo.3 ,

 

I also notice difference in OPP_MODE 

 

So I'm wondering if you have same software version embed in the 2 boards

 

Can you share boot logs of each boards ? 

 

Thanks 

 

Olivier 

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
Technical Moderator
July 11, 2023

Hi @MJo.3 ,

 

I also notice difference in OPP_MODE 

 

So I'm wondering if you have same software version embed in the 2 boards

 

Can you share boot logs of each boards ? 

 

Thanks 

 

Olivier 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MJo.3
MJo.3Author
Associate II
August 11, 2023

I checked software version and it's not same.

I upgrade the os, and it works

 

Thanks