Skip to main content
Visitor II
April 10, 2024
Question

STM32MP255F - High Speed ADC Interface

  • April 10, 2024
  • 1 reply
  • 1196 views

Hello

 

I would like to interface the STM32MP255F to high-speed ADC like AD8285 or MAX1127 using these ADC's parallel interface.

Is it possible to perform such interface while using the STM32MP255F GPIO lines?

 

Thanks.

This topic has been closed for replies.

1 reply

PatrickF
Technical Moderator
April 12, 2024

HI @sem_z ,

the MAX1127 is serial LVDS output and STM32MP25xx product does not have any native interface compatible with that.


For pure HW perspective, the AD8285 should work connected to STM32MP25xx PSSI peripheral inputs.
The max clock for the PSSI RX is not yet listed in the STM32MP25 datasheet, but should be above the maximum rate of the AD8285 (72MHz).

For SW point of view, I'm not sure Cortex-A35/Linux will provide a driver for PSSI (at least not in short term) and what could be the possible system performances under Linux.
Nevertheless, bare-metal HAL for Cortex-M33 includes a PSSI driver.

Regarding SW, you will find more information on those specific STM23MP25 links (as product is still in PreRelease phase)
https://www.st.com/en/microcontrollers-microprocessors/stm32mp2-series/documentation.html?querycriteria=productId=SS2315$$resourceCategory=guides$$resourceType=user_guides#documentation

 

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here