STM32MP257 LPDDR4 routing: Line length from die to ball for STM32MP257 (VFBGA424 package)
Hi,
I'm working on layout routing from STM32MC257AAK(Package: VFBGA424) to LPDDR4 (32bit).
I have read the "Memory layout rules" in the App-Note AN5724.
For a good LPDDR4 signal timing it is usefull to do a "Line-Length-Matching" on the LPDDR4 signals, as noted in the AN5724.
Addidtionally:
For calculating a good "Line-Length-Matching" from MCU to the LPDDR4, I want to know the internal line length from die to ball (Package: VFBGA424).
Could you please provide the internal line length from die to ball (Package: VFBGA424).
Reguards