Skip to main content
Will_Robertson
Associate III
December 17, 2024
Question

STM32MP257 SoM, SiP or SBC

  • December 17, 2024
  • 1 reply
  • 1584 views

Hi,

I was wondering if ST or any ST Partners are planning to produce a System-on-Module (SoM), System-in-Package (SiP) or Single Board Computer (SBC) based on the new STM32MP257 chips?

We're planning to develop using the STM32MP257F-DK evaluation board then find a SoM, SiP or SBC that supports the STM32MP257's MIPI CSI-2 interface and ability to quickly wake from a low power sleep mode.

Will

1 reply

Olivier GALLIEN
Technical Moderator
December 18, 2024

Hi @Will_Robertson 

This is few SOM based on STM32MP257 I can share : 

Digi :  Digi ConnectCore® MP255 CC-WST-J17D-NK

            Digi ConnectCore® MP255 CC-ST-J17D-ZK  

Engicam :  iCore-STM32MP2

              SmarCore-STM32MP2

Myir : MYC-LD25X

Karo : txmp2

Not aware of any SiP or SBC project. 

Hope it help 

Olivier 

 

 

 

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Will_Robertson
Associate III
December 18, 2024

Hi @Olivier GALLIEN 

Thank you very much! I'd been in touch with the two European SoM manufacturers but I hadn't known about digi.com !

Thank you very much also for encouraging me to look at the STM32MP255 instead of the STM32MP257 - I can see now that they're identical except for the STM32MP257 having an Ethernet switch.

We're aiming to design a new open source wildlife camera ecosystem for conservation of endangered Hazel Dormice (Muscardinus avellanarius) and Garden Dormice (Eliomys quercinus) that will use the STM32MP25x μP and ST image sensors to give vastly better performance and be vastly more flexible than anything available at the moment.

Here's a video from our work: Video of Garden Dormouse (Eliomys quercinus) Exploring One of Our Carved Nest Holes https://youtu.be/2mKmhZvdw-4 

and an article (in Flemish but I can translate) Tree Cavities Carved for Endangered Dormice https://www.natuurpunt.be/nieuws/boomholtes-kerven-voor-bedreigde-eikelmuizen 

The system will spend most of its time in a low power sleep mode, wakening to full power when PIR sensors detect an animal approaching so that it can be powered from a solar panel and rechargeable battery. ST's high quality image sensors via a MIPI CSI-2 interface will capture high quality video even in difficult lighting conditions.

I'm a professional climbing arborist and software engineer so OpenST Linux is hugely valuable and the new features in the STM32MP25x μPs are very exciting.

Will