Skip to main content
Associate II
December 19, 2025
Solved

STM32MP257 U-Boot bmp display does not work with MIPI-DSI 1-lane panel

  • December 19, 2025
  • 2 replies
  • 391 views

Product

STM32MP257DAK3 CPU
Board: Custom board (based on STM32MP257)


Software Environment

  • U-Boot: from stm32mp-openstlinux-6.6-yocto-scarthgap-mpu-v25.08.27

  • Boot stage: U-Boot

  • Display command: bmp display

  • Display interface: MIPI-DSI


Problem Description

I am using STM32MP257DAK3 with two different MIPI-DSI LCD panels:

  1. Panel A: MIPI-DSI 4 lanes
    → Works correctly in U-Boot using bmp display

  2. Panel B: MIPI-DSI 1 lane
    → Does NOT work in U-Boot using bmp display

According to the STM32MP25 reference manual, the DSI_PCONFR register supports lane configuration from 1 to 4 lanes.
Therefore, I expect DSI 1-lane mode to be supported by hardware.

However, in U-Boot, the 1-lane panel does not display anything.

SullyNiu_0-1766198950893.png

 

Important Clarification

For both panels:

  • Device Tree is already adapted separately:

    • Correct dsi,lanes = <4> and dsi,lanes = <1> configuration

    • Separate panel nodes

  • Panel drivers are already adapted and validated


Question / Clarification Requested

I would like to confirm:

  1. Does the U-Boot DSI driver (drivers/video/stm32/stm32_dsi.c) officially support MIPI-DSI 1-lane mode?

  2. Is there any limitation, missing configuration, or hard-coded lane setting in the current U-Boot implementation that only supports  4-lane panels?

  3. Is this a known limitation or known issue in the STM32MP25 U-Boot BSP?


Additional Notes

  • The issue is only observed in U-Boot stage when using bmp display.

  • No DSI error is printed in U-Boot console.

  • The DSI PHY and clock configuration are shared between both panels.


Expected Behavior

U-Boot should correctly configure the DSI controller to operate in 1-lane mode.


Request

Please clarify whether:

  • DSI 1-lane mode is supported in U-Boot for STM32MP257

  • A patch or workaround is required

  • Or if this is a known limitation in the current BSP release

Best answer by SullyNiu

Answer

Yes, the U-Boot DSI driver (drivers/video/stm32/stm32_dsi.c) officially supports MIPI-DSI 1-lane mode.

I have successfully brought up a MIPI-DSI 1-lane panel in U-Boot on STM32MP25.
After verification:

  • The DSI host is correctly configured to 1 data lane

  • No hard-coded 4-lane limitation exists in the current U-Boot implementation

  • The issue was not a BSP limitation or known issue

The U-Boot DSI driver works as expected for both 1-lane and 4-lane panels, provided that:

  • Device tree configuration is correct

  • Panel initialization sequence and timing parameters match the panel datasheet

SullyNiu_1-1766366258878.jpeg

 

SullyNiu_0-1766366238948.jpeg

 

2 replies

SullyNiuAuthor
Associate II
December 20, 2025

Ticket Update – Additional Debug Information

I have performed additional debugging in U-Boot by directly reading the DSI registers.

  • Register DSI_PCONFR at address 0x480000A4

  • Value read: 0x00002000

According to the STM32MP25 reference manual, this value corresponds to 1 data lane configuration.

SullyNiu_0-1766196738933.png

 

SullyNiuAuthorBest answer
Associate II
December 22, 2025

Answer

Yes, the U-Boot DSI driver (drivers/video/stm32/stm32_dsi.c) officially supports MIPI-DSI 1-lane mode.

I have successfully brought up a MIPI-DSI 1-lane panel in U-Boot on STM32MP25.
After verification:

  • The DSI host is correctly configured to 1 data lane

  • No hard-coded 4-lane limitation exists in the current U-Boot implementation

  • The issue was not a BSP limitation or known issue

The U-Boot DSI driver works as expected for both 1-lane and 4-lane panels, provided that:

  • Device tree configuration is correct

  • Panel initialization sequence and timing parameters match the panel datasheet

SullyNiu_1-1766366258878.jpeg

 

SullyNiu_0-1766366238948.jpeg