Skip to main content
debugging
Lead
March 20, 2025
Question

STM32MP257F-DK board - No USB DFU mode, Failed to connect STLINK (EMMC2 boots u-boot)

  • March 20, 2025
  • 1 reply
  • 928 views

Found the cause and solved. what happened was:

1. Plugged the host PC only into the STLINK USB-C. with SW1 set to 1, the device booted from EMMC and debug data was shown on USB UART. Assumed based on the MPU running, it would be enough power for the DFU mode.

Once the USB connection was shown in ST CueProgrammer but later on it disappeared and USB connection was never detected again.

2. Bit ofcourse, DFU is not provided via STLINK hardware but via the DRD ,  CPU OTG USB interface. Though after connecting the USB DRD into another USB host connector there was still no DFU mode.

3. After connecting the  STLINK USB-C to an 5V charger and a USB-C cable from  DRD to the host DFU mode came up.

This particular PC might be too old to provide enough juice. but wonder why this board does need more power than a USB-A 3.0 connector  can supply (0.9A) . Perhaps some may run into the same issue.

Cant use DFU mode and ST-LINK at the same time, but the board works.

 

 

1 reply

Visitor II
August 18, 2025

I had the exact same issue. Not sure why it's happening, but can someone please help us?