STM32MP257F-EV1 DDR Firmware Utility: Error “Please specify Binaries path”
- October 8, 2025
- 1 reply
- 485 views
Hello ST Community,
I am working with the STM32MP257F-EV1 Evaluation Board and following the steps described in the official STM32 DDR Firmware Util documentation as per attached document below.
While performing the DDR firmware update and running the DDR utility using STM32CubeProgrammer, I encountered the following issues:
When I try to load the DDR utility binary (STM32MP257F-EV1_DDR_UTILITIES_A35_nopad_no_el3lnch.stm32) and other binaries generated in the process have also been uploaded and downloaded same error as in the attached image we have used DFU mode 0000 and in USB connection is used, STM32CubeProgrammer shows an error message:
“Error: Please specify Binaries path”
for your reference we have attached the image .Environment details:
Board: STM32MP257F-EV1
Connection: USB (DFU mode)
Tool: STM32CubeProgrammer (latest version)
OS: Windows 11
Binary used: STM32MP257F-EV1_DDR_UTILITIES_A35_nopad_no_el3lnch.stm32
Repository: STM32DDRFW-UTIL
Questions:
How can I correctly set the binaries path in STM32CubeProgrammer to avoid the “Please specify Binaries path” error?
- Could there be a configuration or hardware dependency (e.g., jumper or PMIC setting) that I need to verify on the EV1 board?
- Are we missing any key steps in between for this error?
Any guidance or step-by-step clarification would be greatly appreciated.