Skip to main content
RichKnight
Associate II
April 23, 2025
Question

STM32MP257f-ev1 flash error

  • April 23, 2025
  • 0 replies
  • 358 views

Moved from MCUs forum.


RichKnight_0-1745413024014.png

I met this error and can not continue flashing the board. Could any one help me? All configurations are same with https://wiki.stmicroelectronics.cn/stm32mpu/wiki/STM32MP25_Evaluation_boards_-_Starter_Package#Downloading_the_image_and_flashing_it_on_the_board

My board is STM32MP257F-ev1, I just followed the sequence to flash my board, but failed.

RichKnight_1-1745413356098.jpeg

ld5, ld6 and ld11 are lighted when I start with usb/uart boot.

PS: the system is Ubuntu 20.04 on a VirtualBox VM, And I can use Windows to flash the board, and I still can use this VM to flash the SD card with raw image. But the image will no be flashed via Ubuntu on normal flashing with this EVB

 

20250519:

I use windows to flash this board without any problems. But seem I can not use virtualbox based ubuntu 20.04 to flash.