Skip to main content
Visitor II
February 7, 2025
Question

STM32MP257F & Raspberry Camera v2. (IMX219)

  • February 7, 2025
  • 0 replies
  • 846 views

Hello,

For students, we recently bought the STM32MP257F eval board, and the related camera and hdmi bridge.

Everything works perfectly and I would like to connect a Raspberry Camera v2. (IMX219) to the board, as it is also a CSI/MIPI camera (and whe have severals).

Can it work ? what should be done related to the software ? (drivers and so on).

By the way, what is the process to install packages in the board  ?

Best regards

S. M.