Skip to main content
HMüll.4
Senior
March 25, 2025
Solved

STM32MP257F: start some M33 code out of a running Linux?

  • March 25, 2025
  • 1 reply
  • 444 views

Hi,

when the STM32MP257F cores are running a regular Linux: how can I start some code on the M33 core? Is there a device/interface available within Linux that allows to send some code to this core and execute it? Or do they share some memory? So how is it working practically?

Thanks :)

Best answer by Christophe Guibout

Hello @HMüll.4,

 

I would recommand to have a look into Linux remoteproc wiki page : I guess it will help.

BR,

Christophe

1 reply

Christophe Guibout
ST Employee
March 25, 2025

Hello @HMüll.4,

 

I would recommand to have a look into Linux remoteproc wiki page : I guess it will help.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.