Skip to main content
Best answer by PatrickF

Hi @Sharan 

the stm32mp157d-dk1 is not provided with any DSI display, only HDMI screen is possible.
You could connect a display on DSI connector CN4, but you need to found a compatible display (pinout is somewhat compatible with RPi3 for pin 1 to 15, so need to put the flat cable carefully shifted). Then need to adapt the SW with the used display. Using a different display might mean some feature like backlight or touch screen might work differently and need additional SW and HW adaptations.

Maybe more straightforward to use the stm32mp157f-dk2 which come with a DSI display fully supported in the board Starter Package SW.

Regards.

1 reply

PatrickF
PatrickFBest answer
Technical Moderator
September 20, 2024

Hi @Sharan 

the stm32mp157d-dk1 is not provided with any DSI display, only HDMI screen is possible.
You could connect a display on DSI connector CN4, but you need to found a compatible display (pinout is somewhat compatible with RPi3 for pin 1 to 15, so need to put the flat cable carefully shifted). Then need to adapt the SW with the used display. Using a different display might mean some feature like backlight or touch screen might work differently and need additional SW and HW adaptations.

Maybe more straightforward to use the stm32mp157f-dk2 which come with a DSI display fully supported in the board Starter Package SW.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
SharanAuthor
Senior II
September 23, 2024

for the ide can i use stm32cubeide to program or should i need to install linux and if linux how to how to boot the image in sd card?