Skip to main content
JPabl.1
Associate III
November 3, 2024
Solved

STM32MPU157F-DK2 flash process fails after partition 3 reconnects

  • November 3, 2024
  • 2 replies
  • 1161 views

I'm trying to build a linux image for this target. I had successfully(after a lot of trial & error) flashed the target with the Starter package.

For some strange reasons when doing the distribution package, I had to reinstall my VM and now I'm trying again this process. This is the data before downloading

JPabl1_0-1730597142904.png

The problem is that the download process fails at this stage:

JPabl1_1-1730597193281.png

It happens the same with the distribution package with an image I already built I can confirm the "usb gadget" is forwarded to the VM. 

Thanks a lot in advance :)

Best answer by JPabl.1

It seems you can't reflash the starter package, which is what I was trying to do... 

2 replies

PatrickF
Technical Moderator
November 4, 2024

Hi @JPabl.1 

please confirm you use a STM32MP157F-DK2 board with ST Starter Package (and not another board or custom board).

If not related to VM USB link (which is the most frequent cause of 'reconnect' issue), could you share the UART console output (available thru STLink VCP) to see if any errors.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
JPabl.1
JPabl.1AuthorBest answer
Associate III
November 9, 2024

It seems you can't reflash the starter package, which is what I was trying to do...