STM32MPU157F-DK2 issue with flashing the built image with Distribution Package
- April 24, 2023
- 1 reply
- 3326 views
Hey,
I was able to successfully flash the Starter Package following this article and after building the OpenSTLinux distribution following this, I'm having trouble with flashing it. After completeing the build process, inside the flashlayout_st-image-weston, there are 3 folders optee, extensible and deleteall. I was looking for trusted folder like in starter package but it is not available. Then I tried to follow article found here with cube programmer interface and through terminal with FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv but i'm getting following error.
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x05 failed
Error: TSV flashing service failedAfter that I tried to flash with FlashLayout_sdcard_stm32mp157c-dk2-optee.tsv in Starter Package but it also showed the same issue. I have attached the cube programmer terminal output. Apreciate if anyone can help me with this.
Thanks.