Skip to main content
Visitor II
February 12, 2025
Question

The issue of video brightness loss in H264 hardware encoder

  • February 12, 2025
  • 0 replies
  • 538 views

After my video data is encoded by H264 hardware, the picture becomes darker. This issue doesn't occur when displayed directly. Both the ISP and the camera preview are normal. I need some help.

board : stm32mp257f-eval

camera: imx335
hardware encoder parameters : encodebin profile="video/x-h264|element-properties,keyframe-interval=5,rate-control=0,qp-min=20,qp-max=20"