Skip to main content
SRaic.1
Associate
May 22, 2023
Question

UART4 Pins H13 and H14 not working as expected.

  • May 22, 2023
  • 3 replies
  • 1937 views

I am trying to use the UART4 TX: H13 and RX: H14 pins for the tty console access.

The TX from the MPU works fine as I can see the kernel boot logs, but cannot access the kernel command line. No prompt shows up on hitting ENTER.

Here are my stm32mp15-pinctrl.dtsi UART4 configurations:

   uart4_pins_a: uart4-0 {

    pins1 {

      //pinmux = <STM32_PINMUX('G', 11, AF6)>; /* UART4_TX */

      pinmux = <STM32_PINMUX('H', 13, AF8)>;  /* UART4_TX */

      bias-disable;

      drive-push-pull;

      slew-rate = <0>;

    };

    pins2 {

      //pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */

      pinmux = <STM32_PINMUX('H', 14, AF8)>; /* UART4_RX */

      bias-disable;

    };

  };

  uart4_idle_pins_a: uart4-idle-0 {

    pins1 {

      //pinmux = <STM32_PINMUX('G', 11, ANALOG)>; /* UART4_TX */

      pinmux = <STM32_PINMUX('H', 13, ANALOG)>;  /* UART4_TX */

    };

    pins2 {

      //pinmux = <STM32_PINMUX('B', 2, AF8)>; /* UART4_RX */

      pinmux = <STM32_PINMUX('H', 14, AF8)>; /* UART4_RX */

      bias-disable;

    };

  };

  uart4_sleep_pins_a: uart4-sleep-0 {

    pins {

      //pinmux = <STM32_PINMUX('G', 11, ANALOG)>, /* UART4_TX */

      //  <STM32_PINMUX('B', 2, ANALOG)>; /* UART4_RX */

      pinmux = <STM32_PINMUX('H', 13, ANALOG)>, /* UART4_TX */

         <STM32_PINMUX('H', 14, ANALOG)>; /* UART4_RX */

    };

  };

And the stm32mp15xx-evx.dtsi configurations:

&uart4 {

  pinctrl-names = "default", "sleep", "idle";

  pinctrl-0 = <&uart4_pins_a>;

  pinctrl-1 = <&uart4_sleep_pins_a>;

  pinctrl-2 = <&uart4_idle_pins_a>;

  //uart-has-rtscts;

  //status = "disabled";

  status = "okay";

};

Have also added chosen path as:

   chosen {

    stdout-path = "serial0:115200n8";

  };

  aliases {

    serial0 = &uart4;

  };

What is missing for the configurations?

This topic has been closed for replies.

3 replies

Kevin HUBER
Technical Moderator
May 26, 2023

Hello @SRaic.1​ ,

Please can you share the complete boot log.

Does it was working previously with the default UART4 config?

Does it work under U-Boot?

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
SRaic.1
SRaic.1Author
Associate
May 27, 2023

Hi @Kevin HUBER​ 

Attaching boot logs after enabling the UART 4 as console uart.

Yes, when using the default uart4 config, uart4 TX and RX worked fine as kernel console.

Not made changes for U-boot uart4 yet.

Regards,

Swapnil.

Kevin HUBER
Technical Moderator
May 29, 2023

Hello @SRaic.1​ ,

You are using an ecosystem v2.1 that is no longer supported by ST (deprecated version), it is recommended to switch to the latest environment release which is the v4.1:

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_OpenSTLinux_release_note_-_v4.1.0

Otherwise, regarding your problem I tried on my 157F-EV1 board with the ecosystem v4.1.0 and I was able to use H13 and H14 without issue.

It is possible to verify which pins are used with the command:

root@stm32mp1:~# cat /sys/kernel/debug/pinctrl/soc:pinctrl@50002000/pinmux-pins
 
pin 125 (PH13): device 40010000.serial function af8 group PH13
pin 126 (PH14): device 40010000.serial function af8 group PH14

For doing that I only modified (for test purpose) the file stm32mp15-pinctrl.dtsi

where I replaced every

  • "('G', 11, AF6)" by "('H', 13, AF8)"
  • "('B', 2, AF8)" by "('H', 14, AF8)"

In uart4_pins_a,  uart4_idle_pins_a, uart4_sleep_pins_a.

I didn't changed anything else.

My uart4 node looks like this:

&uart4 {
	pinctrl-names = "default", "sleep", "idle";
	pinctrl-0 = <&uart4_pins_a>;
	pinctrl-1 = <&uart4_sleep_pins_a>;
	pinctrl-2 = <&uart4_idle_pins_a>;
	/delete-property/dmas;
	/delete-property/dma-names;
	status = "okay";
};

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here