Skip to main content
Associate
November 14, 2025
Question

USB3DR Peripheral Mode on STM32MP257F-DK

  • November 14, 2025
  • 3 replies
  • 187 views

Hi all,

I'm trying to get a USB Gadget device working in Linux on the STM32MP257F-DK board to expose a Mass Storage device to another system. I'm trying to use CN15 for this function but I can't get the bound gadget to show up on the other side of the USB connection.

I'm using a fork of github.com/STMicroelectronics/linux?branch=v6.6-stm32mp where I've modified the usb3dr node of the dk.dts file with the following things:

1. 

836	&usb3dr {
837		status = "okay";
838
839		dwc3: usb@48300000 {
840			phys = <&usb2_phy2>, <&combophy PHY_TYPE_USB3>;
841			phy-names = "usb2-phy", "usb3-phy";
842			usb-role-switch;
843			dr_mode = "peripheral";
844			port {
845				dwc3_ep: endpoint {
846					remote-endpoint = <&typec_ep>;
847				};
848			};
849		};
850	};
2. 
840 -	phys = <&usb2_phy2>, <&combophy PHY_TYPE_USB3>;
841 -	phy-names = "usb2-phy", "usb3-phy";
842 840	usb-role-switch;
843 -	dr_mode = "peripheral";
841 +	role-switch-default-mode = "peripheral";
841 +	maximum-speed = "high-speed";​

3. 

843 +	
844 +	dr_mode = "peripheral";

4.

844 -	dr_mode = "peripheral";
844 +	dr_mode = "otg";

I've also validated that my hardware connection works by booting into serial downloader boot mode, in which case I've been able to see the `STMicroelectronics STM Device in DFU Mode`.

I did come across this post: https://community.st.com/t5/stm32-mpus-products-and-hardware/stm32mp257dak3-usb3dr-not-working-in-peripheral-mode-under-linux/m-p/796776
It seems like a similar, if not the same issue, but they don't actually detail what they did to the u-boot device tree to make it work. 

Anyway, I'd appreciate any help anyone is willing to give!

Justin

3 replies

PatrickF
Technical Moderator
November 17, 2025

Hi @jseely 

 

Have you looked to https://wiki.st.com/stm32mpu/wiki/USB3DR_device_tree_configuration

 

Any significant message on the board console during boot (dmesg) ?

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.NEW ! Sidekick STM32 AI agent, see here
jseelyAuthor
Associate
November 17, 2025

Hi Patrick,

Thanks for the reply. Yes I have been looking at that, that has been where most of the things I have tried have come from.

As for the dmesg logs:

root@evb-stm32mp257f-dk:~# dmesg | grep -i "usb\|udc\|48300000" 
[ 0.798737] /ahb@1/i2c@2/typec@35/connector: Fixed dependency cycle(s) with /soc@0/bus@42080000/usb@48300000/usb@48300000
[ 0.806632] /ahb@1/i2c@2/typec@35/connector: Fixed dependency cycle(s) with /soc@0/bus@42080000/usb@48300000/usb@48300000
[ 0.953126] usbcore: registered new interface driver usbfs
[ 0.958226] usbcore: registered new interface driver hub
[ 0.963501] usbcore: registered new device driver usb
[ 1.449341] usbcore: registered new interface driver usb-storage
[ 1.453385] usbcore: registered new device driver onboard-usb-hub
[ 1.506124] usbcore: registered new interface driver usbhid
[ 1.511024] usbhid: USB HID core driver
[ 1.734535] scmi-regulator scmi_dev.6: Regulator vdd3v3_usb registered for domain [20]
[ 2.262802] usb-stm32-dwc3 42080000.bus:usb@48300000: configured in usb3 mode
[ 2.265181] /ahb@1/i2c@2/typec@35/connector: Fixed dependency cycle(s) with /soc@0/bus@42080000/usb@48300000/usb@48300000
[ 2.275406] /soc@0/bus@42080000/usb@48300000/usb@48300000: Fixed dependency cycle(s) with /ahb@1/i2c@2/typec@35/connector
[ 2.289522] UDC core: USB initialize gadget.
[ 2.291658] UDC core: USB add gadget.
[ 2.294142] UDC core: USB gadget state set to 0.
[ 2.300571] UDC core: USB gadget state work scheduled.
[ 12.767092] stm32mp_pm_domain power-domain-d1: sync_state() pending due to 42080000.bus:usb@482e0000
[ 3809.622873] UDC core: USB gadget register driver owner requested.
[ 3809.623592] UDC core: USB gadget bind driver requested.
[ 3809.628717] UDC core: UDC set speed to 5.
[ 3809.645393] udc 48300000.usb: failed to start g_mass_storage: -22
[ 3809.657816] UDC core: g_mass_storage: couldn't find an available UDC
[ 3894.290040] UDC core: USB gadget register driver owner requested.
[ 3894.290705] UDC core: USB gadget bind driver requested.
[ 3894.296047] UDC core: UDC set speed to 5.
[ 3894.300783] UDC core: USB gadget enable async callbacks.
[ 3894.305138] UDC core: USB gadget connect control locked.
[ 3894.310917] UDC core: USB gadget connect requested.

For context 3809 is where I `modprobe g_mass_storage` and 3894 is where I run the following script:

#!/usr/bin/env bash
set -eux

image=/home/root/usb.img
dd if=/dev/zero of=${image} bs=1MB count=25

usbdev_configfs=/sys/kernel/config/usb_gadget
gadget_dir=${usbdev_configfs}/mass-storage-test

mkdir ${gadget_dir}
cd ${gadget_dir}

echo 0x1d6b > idVendor
echo 0x0104 > idProduct

strings_dir=${gadget_dir}/strings/0x409
mkdir -p ${strings_dir}

echo "OpenBMC" > ${strings_dir}/manufacturer
echo "Virtual Media Device (test)" > ${strings_dir}/product

config_strings_dir="${gadget_dir}/configs/c.1/strings/0x409"
mkdir -p ${config_strings_dir}

echo "config 1" > ${config_strings_dir}/configuration

func_mass_storage_dir="${gadget_dir}/functions/mass_storage.usb0"
lun0="${func_mass_storage_dir}/lun.0"
mkdir -p ${lun0}

echo 1 > ${lun0}/removable
echo 0 > ${lun0}/ro
echo 0 > ${lun0}/cdrom
echo ${image} > ${lun0}/file

ln -s ${func_mass_storage_dir} "${gadget_dir}/configs/c.1/mass_storage.usb0"

Most of the UDC core log messages are messages I placed inside `drivers/usb/dwc3/core.c` in the linux kernel to help with debugging.

 

Is there some way that the earlier boot layers could be restricting access to the memory regions I would need to configure the UDC on this port, specifically some way that linux wouldn't complain about when configured to use them?

Sorry I'm still very new to this chip!

Justin

 

Associate
March 20, 2026

I am seeing this same issue. DWC3 appears to be in gadget mode, but nothing is showing up on my usb host side.

 # ls /sys/kernel/debug/usb/48300000.usb/
ep0in ep11out ep3in ep5out ep8in lsp_dump
ep0out ep1in ep3out ep6in ep8out regdump
ep10in ep1out ep4in ep6out ep9in testmode
ep10out ep2in ep4out ep7in ep9out
ep11in ep2out ep5in ep7out link_state

I have tried with both the out of the box reference image (using the /sbin/stm32_usbotg_eth_config.sh script) and a custom built image with a similar usb mass storage script.

 What steps are needed to enable USB gadget functionality on this board?