Skip to main content
Associate
November 15, 2023
Question

VirtIO problem on STM32MP157C-DK2

  • November 15, 2023
  • 3 replies
  • 2540 views

Hi! I am working with stm32mp157c-dk2 and trying to establish communication between m4 and a7 cores. I analyze standard examples for this purpose, namely OpenAMP_TTY_echo. VIRT_UART initialization is presented here for m4 core:

 

 

log_info("Virtual UART0 OpenAMP-rpmsg channel creation\r\n");
 if (VIRT_UART_Init(&huart0) != VIRT_UART_OK) {
 log_err("VIRT_UART_Init UART0 failed.\r\n");
 Error_Handler();
 }

 log_info("Virtual UART1 OpenAMP-rpmsg channel creation\r\n");
 if (VIRT_UART_Init(&huart1) != VIRT_UART_OK) {
 log_err("VIRT_UART_Init UART1 failed.\r\n");
 Error_Handler();
 }

 /*Need to register callback for message reception by channels*/
 if(VIRT_UART_RegisterCallback(&huart0, VIRT_UART_RXCPLT_CB_ID, VIRT_UART0_RxCpltCallback) != VIRT_UART_OK)
 {
 Error_Handler();
 }
 if(VIRT_UART_RegisterCallback(&huart1, VIRT_UART_RXCPLT_CB_ID, VIRT_UART1_RxCpltCallback) != VIRT_UART_OK)
 {
 Error_Handler();
 }

 

After flashing is issued:

 

[ 111.672943] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 111.678249] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 111.685266] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 111.690252] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[ 111.696384] remoteproc remoteproc0: remote processor m4 is now up
[ 115.293405] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x0
[ 115.299594] virtio_rpmsg_bus virtio0: channel rpmsg-tty-channel:ffffffff:0 already exist
[ 115.307771] virtio_rpmsg_bus virtio0: rpmsg_create_channel failed
[ 115.313773] virtio_rpmsg_bus virtio0: creating channel rpmsg-tty-channel addr 0x1
[ 115.321384] virtio_rpmsg_bus virtio0: channel rpmsg-tty-channel:ffffffff:1 already exist
[ 115.329519] virtio_rpmsg_bus virtio0: rpmsg_create_channel failed

 

And when viewing tty:

 

root@stm32mp1:~# ls /dev/tty*
/dev/tty /dev/tty2 /dev/tty31 /dev/tty43 /dev/tty55 /dev/ttySTM0
/dev/tty0 /dev/tty20 /dev/tty32 /dev/tty44 /dev/tty56 /dev/ttyp0
/dev/tty1 /dev/tty21 /dev/tty33 /dev/tty45 /dev/tty57 /dev/ttyp1
/dev/tty10 /dev/tty22 /dev/tty34 /dev/tty46 /dev/tty58 /dev/ttyp2
/dev/tty11 /dev/tty23 /dev/tty35 /dev/tty47 /dev/tty59 /dev/ttyp3
/dev/tty12 /dev/tty24 /dev/tty36 /dev/tty48 /dev/tty6 /dev/ttyp4
/dev/tty13 /dev/tty25 /dev/tty37 /dev/tty49 /dev/tty60 /dev/ttyp5
/dev/tty14 /dev/tty26 /dev/tty38 /dev/tty5 /dev/tty61 /dev/ttyp6
/dev/tty15 /dev/tty27 /dev/tty39 /dev/tty50 /dev/tty62 /dev/ttyp7
/dev/tty16 /dev/tty28 /dev/tty4 /dev/tty51 /dev/tty63
/dev/tty17 /dev/tty29 /dev/tty40 /dev/tty52 /dev/tty7
/dev/tty18 /dev/tty3 /dev/tty41 /dev/tty53 /dev/tty8
/dev/tty19 /dev/tty30 /dev/tty42 /dev/tty54 /dev/tty9

 

As You can see in /dev/tty* the /dev/ttyRPMSG0 port is not created on the A7 kernel side. Can you please tell me what step I am missing? Thanks in advance!

This topic has been closed for replies.

3 replies

Erwan SZYMANSKI
Technical Moderator
November 16, 2023

Hello @Ljubica ,
Can you please give me the Cube_FW_package version that your are using, as well as the OpenSTLinux version that you use.

Do you use the Starter package to get the SW image ? 

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LjubicaAuthor
Associate
November 20, 2023

Thank you for reply, @Erwan SZYMANSKI ,
I am using STM32Cube_FW_MP1_V1.6.0 -> Projects -> STM32MP157C-DK2 -> Applications -> OpenAMP -> OpenAMP_TTY_echo with STM32MP1 OpenSTLinux 4.1.0 startup package.

Erwan SZYMANSKI
Technical Moderator
November 20, 2023

@Ljubica ,
Thanks or the confirmation, versions look aligned. Can you precise following point :

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
LjubicaAuthor
Associate
November 20, 2023

@Erwan SZYMANSKI ,
The STM32MP157C-DK2 is being used, I was doing an early startup without specifying a new path. I'm not quite clear on how to flash without auto startup and how much of an impact it might have?

Kind regards,

Ljubica.

Erwan SZYMANSKI
Technical Moderator
November 20, 2023

@Ljubica ,
I have already seen people who have trouble with co-processor early startup. I just would like to confirm that it can work at runtime and that channels are well created. For this, on Linux side, you can use the link on the wiki I gave you to check if it works or not.

Second question concerning the use case. Do you need to do early work on M4 side ? What I want to highlight is that, if you do not need M4 cortex very early in the boot process, maybe the easier way is to start the M4 firmware (the Echo program here) only when Linux boot is finished.

Kind regards,
Erwan. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.