When we use the PMIC values from DK2 example.
1 . ERROR: regul ldo3: max value 750 is invalid
WARNING: register_pmic:600 failed to register ldo3
PANIC at PC : 0x2fff05cb
2 Next we tried setting the ldo3 max, min values to 3V and 1.8V and it was working fine but had next layer of issue as mentioned below.
NOTICE: CPU: STM32MP157AAD Rev.Z
NOTICE: Model: MelodySOM
INFO: PMIC version = 0x21
WARNING: VDD unknown
NOTICE: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r1.0(debug):v2.6-dirty
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000kHz
ERROR: DDR addr bus test: can't access memory @ 0xc0000004
PANIC at PC : 0x2ffead6d
Exception mode=0x00000016 at: 0x2ffead6d
Requesting for your help to solve this as soon as possible.