Skip to main content
JPabl.1
Associate III
November 9, 2024
Solved

yocto image fails for stm32mp15-disco

  • November 9, 2024
  • 1 reply
  • 1007 views

I created a qt quick app onqt  version 6.7.3 for the stm32mp157f-disco. 

I was able to test using qt creator and boot 2 qt on the target board and it worked just fine. 

Now, I'm in process of building the linux image for the target. Since I don't fully understand how to use yocto, and it seems there's no support from st side for qt on stm32mp15, I decided to go the other path, using the boot 2 qt. 

I created a custom recipe with my qt app and was able to bitbake this recipe. Now, I'm trying to build the entire image but I'm getting the following error:

 

| cd /home/vboxuser/yocto/build-stm32mp15-disco/tmp/work/cortexa7t2hf-neon-vfpv4-poky-linux-gnueabi/qtwebengine/6.7.3/build/src/core && /home/vboxuser/yocto/build-stm32mp15-disco/tmp/work/cortexa7t2hf-neon-vfpv4-poky-linux-gnueabi/qtwebengine/6.7.3/recipe-sysroot-native/usr/bin/ninja -C /home/vboxuser/yocto/build-stm32mp15-disco/tmp/work/cortexa7t2hf-neon-vfpv4-poky-linux-gnueabi/qtwebengine/6.7.3/build/src/core/Release/arm QtWebEngineCore
| ninja: build stopped: subcommand failed.
| 
| WARNING: exit code 1 from a shell command.
ERROR: Task (/home/vboxuser/yocto/sources/meta-qt6/recipes-qt/qt6/qtwebengine_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 8110 tasks of which 7847 didn't need to be rerun and 2 failed.
NOTE: Build completion summary:
NOTE: do_populate_sysroot: 0.0% sstate reuse(0 setscene, 16 scratch)
NOTE: do_deploy_source_date_epoch: 0.0% sstate reuse(0 setscene, 13 scratch)
NOTE: do_create_spdx: 0.0% sstate reuse(0 setscene, 15 scratch)
NOTE: do_create_runtime_spdx: 0.0% sstate reuse(0 setscene, 15 scratch)
NOTE: do_package_qa: 0.0% sstate reuse(0 setscene, 9 scratch)
NOTE: do_recipe_qa: 0.0% sstate reuse(0 setscene, 15 scratch)
NOTE: do_package: 0.0% sstate reuse(0 setscene, 10 scratch)
NOTE: do_packagedata: 0.0% sstate reuse(0 setscene, 10 scratch)
NOTE: do_package_write_ipk: 92.6% sstate reuse(125 setscene, 10 scratch)
NOTE: do_populate_lic: 0.0% sstate reuse(0 setscene, 13 scratch)

Summary: 2 tasks failed:
 /home/vboxuser/yocto/sources/meta-boot2qt/meta-boot2qt/recipes-qt/boot2qt-addons/boot2qt-demolauncher_git.bb:do_unpack
 /home/vboxuser/yocto/sources/meta-qt6/recipes-qt/qt6/qtwebengine_git.bb:do_compile
Summary: There were 6 WARNING messages.
Summary: There were 2 ERROR messages, returning a non-zero exit code.

 

I'm using boot2qt 6.7.3 manifest and MACHINE=stm32mp15-disco and image b2qt-embedded-qt6-image. 

I'm using meta-qt6 layers and the nanbield meta-st layer which is the one that matches. 

This is my bb file in my custom recipe(which builds ok if I only bitbake the custom recipe)

 

SUMMARY = "This is the GUI for Hespect Software medical device"
DESCRIPTION = "Recipe created by bitbake-layers"
LICENSE = "CLOSED"
SECTION = "Mysection"

DEPENDS += " qtbase \
 qtdeclarative-native \
 qtdeclarative \
 qtquick3d \
 qtcharts"
 
RDEPENDS_${PN} += "qtwayland"

EXTRA_OECMAKE += "-DCMAKE_PREFIX_PATH=${STAGING_DIR_HOST}${prefix}"

SRC_URI += "file://main.cpp"
SRC_URI += "file://CMakeLists.txt"
SRC_URI += "file://CMakeLists.txt.user"
SRC_URI += "file://Backendsensors.h"
SRC_URI += "file://Backendsensors.cpp"
SRC_URI += "file://brushfactory.h"
SRC_URI += "file://brushfactory.cpp"
SRC_URI += "file://Main.qml"

# Add SVG images from the assets/images folder
SRC_URI += "file://assets/images/battery-full.svg"
SRC_URI += "file://assets/images/battery-mid.svg"
SRC_URI += "file://assets/images/rss-low.svg"
SRC_URI += "file://assets/images/signal-full.svg"
SRC_URI += "file://assets/images/signal-mid.svg"
SRC_URI += "file://assets/images/battery-low.svg"
SRC_URI += "file://assets/images/rss-full.svg"
SRC_URI += "file://assets/images/rss-mid.svg"
SRC_URI += "file://assets/images/signal-low.svg"

 
S = "${WORKDIR}"

inherit qt6-cmake
inherit populate_sdk_qt6

 

I have no idea what to do next. If this is possible to do starting the yocto environment from a st manifest I would be happy to change to it. 

Best answer by JPabl.1

I tried building the image with the st way and I was able to add the x-linux-qt package to the stm32mp157d-fk2 board and flash the board using the dd command from linux for the microsd card. 

 

I'm having problems finding my custom recipe in the full image but I will post that question on another post. 

1 reply

JPabl.1
JPabl.1AuthorBest answer
Associate III
November 12, 2024

I tried building the image with the st way and I was able to add the x-linux-qt package to the stm32mp157d-fk2 board and flash the board using the dd command from linux for the microsd card. 

 

I'm having problems finding my custom recipe in the full image but I will post that question on another post.