Cannot connect DK1 board via ST-LINK with Keil-MDK
New board STM32MP157A-DK1 bought, trying to connect. First, ST-LINK drivers were updated, then on-board ST-LINK version was updated to last available V2J26M36. MDK cannot connect ("No target connected"), st-link utility cannot see board ("Detection fail"). Through some experiments, by the moment, assume this:
- Oscilloscope shows signals on SWDIO, SWCLK, NRST.
- Tried all available firmware versions (V32...V36) from the site.
- Wires were soldered to TP3, TP5, etc. to got connection to external ST-link. Initially, external ST-LINK/V2 had version M28 and MDK has read ident from the device! But MDK cannot flashing board ("invalid ROM table"), and firmware in external ST-LINK were updated. Since this, it came to the situation "No target connected" which was with the on-board st-Link. Another firmware versions were tried with the same result.
ST-LINK/V2 and ST-LINK/V2 Isol were tried.
In MDK dialog, internal st-link version shows as V2x36x26, but there NO such format in RN0093 doc. Only J36M26 or S7 but no "x". External ST-link version shows correctly, e.g. V2J34S7. What may be wrong?