Cannot recognize device when connected to STM32cubeprogrammer
I have set up the device, 5V 3A wall PSU and connected to the USB stlink connection. Connecting to the onboard stlink I can recognize the board serial number but the programmer fails to recognize the device. What am I missing? The device works perfectly in stand alone mode. As it would not identify the device I upgraded the firmware to V2J37M26 to see if that would correct it.
This was the output in the programmer if it helps.
12:26:58 : ST-LINK SN : 0669FF333536414257062332
12:26:58 : ST-LINK FW : V2J37M26
12:26:58 : Board : --
12:26:58 : Voltage : 3.27V
12:26:58 : SWD freq : 4000 KHz
12:26:58 : Connect mode: Normal
12:26:58 : Reset mode : Hardware reset
12:26:58 : Error: Cannot identify the device