Skip to main content
darla14
Associate III
May 30, 2022
Question

Clarification on the folder structure for CM4 project created by the STM32CubeMX

  • May 30, 2022
  • 1 reply
  • 848 views

Hello,

I see two folders with the same name(STM32MP1xx_HAL_Driver) - one inside the CM4 and another one level above it.

For the development of CM4 which folder to consider for the drivers?

If it is the one inside the CM4 do I need to move the CMSIS as well inside it?

Same question for the middleware folder, which one to be considered? the one inside the CM4 or outside it? I see that enabling any Middleware component it generates the source code inside both the Middleware folder.(e.g Free RTOS)

Br,

D

This topic has been closed for replies.

1 reply

Olivier GALLIEN
Technical Moderator
May 31, 2022

Hi @darla14​ ,

I assume you generate a project for STM32CubeIDE right ?

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
darla14
darla14Author
Associate III
May 31, 2022

Hello @Community member​  ,

Yes correct!

Br,

D