Enable analyzers on the CubeIDE
Hi there,
I'm working on a STM32MP135 project.
I'd like to see some information on the Build Analyzer and/or Static stack analyzer but they always report the grids empty.
The project is compiled with the -fstack-usage and debualt Debug level (-g).
I checked that for each source files of the project are generated the .cyclo, .su, .d and .o files in the Debug directory.
The analyzers windows do not have a button to associate the project: but it seems not to be a problem with the latest relases.
So, why I cannot browse the analyzers data?
Version: 1.19.0
Build: 25607_20250703_0907 (UTC)
Thanks, regards