Skip to main content
Associate III
July 8, 2025
Question

How do I flash (download) an STM32MP157f-dk image created from IOC build?

  • July 8, 2025
  • 1 reply
  • 393 views

I created an STM project of the STM32MP157f-dk2 in eclipse.

smanger_0-1752001029479.png

I've tried to build the entire A7 core linux code. How do I replace what's on the dk2 now? The dk2 just has the starter package on it.

1 reply

smangerAuthor
Associate III
July 8, 2025

I noticed that when I build the linux kernel, the output goes to:

 gcnano-driver-stm32mp-6.4.19-stm32mp1-r1-rc8-r0 -> STM32MPU-Ecosystem-v6.0.0/Developer-Package/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.19-stm32mp1-r1-rc8-r0
linux-6.6.48 -> STM32MPU-Ecosystem-v6.0.0/Developer-Package/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.6.48-stm32mp-r1-r0/linux-6.6.48
Makefile.ide -> STM32MPU-Ecosystem-v6.0.0/Developer-Package/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.6.48-stm32mp-r1-r0/linux-6.6.48/../Makefile.ide

 I try following the same steps as building and copying linux kernel.

When it comes to the following step:

find ${OUTPUT_BUILD_DIR}/arch/${ARCH}/boot/dts/ -name 'st*.dtb' -exec cp '{}' ${OUTPUT_BUILD_DIR}/install_artifact/boot/ \;

there are not any `dtb` files.

Associate II
July 14, 2025

most likely you built into source directory. have a look into linux-6.6.48/arch/arm64/boot/dts