How to register the MAC address of my own board which STM32MP151CAA3 is mounted on?
I want to register the MAC address of my own board which STM32MP151CAA3 is mounted on.
Can I use STM32CubeProgrammer to register the MAC address?
If so, are the following commands correct?
Example)
MAC address which I want to register: 00:12:34:56:78:90
> STM32_Programmer_CLI -c port=usb1 -otp program wordID=0x39 value=0x56341200
> STM32_Programmer_CLI -c port=usb1 -otp program wordID=0x3A value=0x00009078Also, can I update this OTP bits only once?
(If I register the MAC address once, Can't I update it again?)
Best regards
H. Masuda