If HSEM_CnIER registers of STM32MP2 have global access attribute?
Hi,
In STM32MP25x Reference manual(RM0457), the HSEM_(S)Cnxxx registers all have the description of global access attribute except HSEM_CnIER,
as shown of HSEM_CnICR,
22.5.4 HSEM non-secure interrupt clear register (HSEM_CnICR)
Address offset: 0x104 + 0x010 * (n - 1), (n = 1 to 3)
Reset value: 0x0000 0000
Register global access: When CID filtering for processor[n] is enabled in
HSEM_CnCIDCFGR, this register can be accessed only by the processor CID. An illegal
CID access to this register generates a CID illegal access event. When CID filtering for
processor[n] is disabled this register can be accessed by any bus master.
the HSEM_SCnIER also have the description of global access attribute, and the bits of HSEM_CnIER register also have CID filtering access attribute, and all bits maybe could be used by one CID , So if HSEM_CnIER also have the global access attribute?