OpenStLinux 3.0 plugin for Stm32cubeIDE 1.16.1
Hi,
I have to use OpenStLinux 3.0 Developer SDK for my project.
I am using stm32cubemx 6.3.0 to generate the project files.
I then use Stm32cubeide 1.16.1 to import the project.
I was able to specify the location of the installed Developer SDK package 3.0.
However, when I proceed to install the OpenStLinux 3.0 source codes plugin, the IDE will just crush!!!!
Just to confirm, I read on the wiki that Stm32cubeIDE 1.16.1 will import and support Developer SDK package 3.0.
Anyone can help?
Thanks