STLINK-V3SET connection to STM32MP157C using CubeProgrammer
hello,
I am connecting the STM32MP157C to the debugger using STDC14 CN1 connector in JTAG mode.
Please tell me the pin/signal direction, with regard to the debugger, for the following:
Pin 4, T_JTMS
Pin 6, T_JCLK
Pin 8, T_JTDO
Pin 10, T_JTDI
The connection fails using the CubeProgrammer.
I get the following message: "ST-LINK error (DEV_UNKNOWN_MCU_TARGET)".
On the debugger the PWR led lights green and the COM led lights red.
The signals I am using to connect are: T_JTMS, T_JTCK, T_JTDI, T_JTDO (STM32MP157C to debugger) and also providing 3.3V to pin 3, T_VCC and of-course connecting the GND pins.
I am not connecting STM32MP NJTRST pin to pin 12, T_NRST in the debugger (the STM32MP has an internal PU on it).
The STM32MP157C boot mode is JTAG (although doesn't work in USB boot mode).
What am I missing here?
thanks
Gil