Question
STM32CubeIDE 1.17.0 released
We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available.
What is new in 1.17.0:
- Microcontrollers, microprocessors, and board lists aligned with STM32CubeMX:
- Added the support for the STM32N6 series
- Added the support for the STM32U3 series.
- Added the support for the STM32WL3x line
- Added the support for the STM32MP23xx microprocessors
- Added the support for the STM32MP25xx microprocessors in a TFBGA361 16 mm × 16 mm package
- Added the support for new microcontrollers in the STM32C0 series and related Nucleo boards (NUCLEO-C051C8 and NUCLEO-C092RC)
- Added the support for new microcontrollers in the STM32G4 series
- Added the support for new microcontrollers in the STM32WBA series and the related B-WBA5M-WPAN board
- Simplified user authentication interface
- Added support for debug authentication with password for the STM32N6 series.
- Improved support of OpenSTLinux plugin to be version agnostic
- Enabled the installation of both STM32MP1 and STM32MP2 flavors of OpenSTLinux plugins within the same STM32CubeIDE instance.
- Added support for flashing the .bin file during debugging.
Main fixed issues in 1.17.0:
Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata
Known problems and limitations in 1.17.0:
Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata
How to get STM32CubeIDE 1.17.0:
- Under this link
- Or update your current installation of STM32CubeIDE using: Help > Check for updates (The in-tool update does not allow updating the drivers and ST-LINK server tool. Full installation is required for this to be done).