STM32CubeIDE 1.19.0 released
We are pleased to announce that the release 1.19.0 of STM32CubeIDE is available.
What is new in 1.19.0:
- Microcontroller, microprocessor, and board lists aligned with STM32CubeMX v6.15.0:
- Added the support for STM32MP21xx microprocessors to the STM32MP2 series and extended the support for boards based on the STM32MP2 microprocessors
- Added the support for STM32WL30xx and STM32WL31xx microcontrollers to the STM32WL3x line
- Added automatic external memory loader prefilling in debug configuration for boards based on the STM32N6 series
- Added the support for OpenSTLinux 6.1.0 through the update site mechanism
- Added the support for STM32MP2x-M33-TD projects generated from STM32CubeMX standalone
- Added the Cortex®-A35 support in the SFRs view
- Added the capability to install OpenSTLinux through the update site mechanism on empty projects for STM32MP1 and STM32MP2 devices
- Added the support for TF‑M projects debugging for STM32MP2x-M33-TD
- Added the new view Flash memories programming allowing the programming of a TSV file for STM32MP1 and STM32MP2 devices in single or dual storage
- Added the support for new reset strategies when debugging with SEGGER J-Link
- Added incremental programming as an experimental feature for a defined set of devices:
- Internal flash memory programming is tested on the following microcontrollers:
STM32C03xxx, STM32C05xxx, STM32C09xxx, STM32F101/F102/F103, STM32F37xxx,
STM32F411xC/E, STM32F72xxx, STM32F73xxx, STM32F76xxx, STM32F77xxx, STM32G03xxx,
STM32G04xxx, STM32G0B0xx/B1xx/C1xx, STM32G491xx, STM32H50xxx, STM32H523/533,
STM32H562, STM32H563/573, STM32H723/STM32H733, STM32H725/STM32H735, STM32H730
Value line, STM32H7R3/7S3, STM32H7R7/7S7, STM32L05xxx/L06xxx/L010xx, STM32L4P5/Q5,
STM32L4x1, /STM32L475xx/STM32L476xx/STM32L486xx, STM32L5, STM32U0, STM32U3,
STM32U535/545, STM32U575/585, STM32U595/5A5, STM32U599/5A9, STM32WB35xx/5xxx,
STM32WBA52, STM32WBA54/55, STM32WBA62, STM32WBA63, STM32WBA64/65, and
STM32WL - External flash memory programming is tested on the following boards:
STM32H735G-DK, STM32H7S78-DK, STM32H573I-DK and STM32U575I-EV
Main fixed issues in 1.19.0:
Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x
Known problems and limitations in 1.19.0:
Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.19.x
How to get STM32CubeIDE 1.19.0:
- Under this link
- Or update your current installation of STM32CubeIDE using: Help > Check for updates (The intool update does not allow updating the drivers and STLINK server tool. Full installation is required for this to be done).