STM32CubeIDE can't setup OpenSTLinux
I've set the root path in the OpenSTLinux SDK manager, but when I try to download scarthgap from the 'install other software' dialog, it appears to download the SDK, but it never shows up. It's not at the path I specified either. I don't know where, or even if, it actually gets downloaded. When I try to setup openstlinux with the project, I always get an error that it failed to configure openstlinux with scarthgap. I'm assuming that's what's compatible with CubeIDE right now.
CubeIDE thinks it's installed though, it is hidden when I hide the items that are already installed. I've tried this on a Linux VM as well as WSL2 and the behavior is the same.