STM32CubeIDE sample program compiling error
Hi,
I try to compile "OpenAMP_TTY_echo_CM33_NonSecure" sample program as suggested here:
Compiling does not work, I get error message:
0:43:14 **** Build of configuration CA35TDCID_m33_ns_sign for project OpenAMP_TTY_echo_CM33_NonSecure ****
make -j16 all
cmake -S ../../../../../../../../../Middlewares/Third_Party/OpenAMP/libmetal/ -B libmetal -G"Unix Makefiles" -DCMAKE_TOOLCHAIN_FILE=cmake/platforms/stm32mp-generic-gcc.cmake
CMake Error at CMakeLists.txt:1 (cmake_minimum_required):
-- Configuring incomplete, errors occurred!
Compatibility with CMake < 3.5 has been removed from CMake.
Update the VERSION argument <min> value. Or, use the <min>...<max> syntax
to tell CMake that the project requires at least <min> but has been updated
to work with policies introduced by <max> or earlier.
Or, add -DCMAKE_POLICY_VERSION_MINIMUM=3.5 to try configuring anyway.
make[1]: *** [makefile:104: pre-build] Error 1
make: *** [makefile:72: all] Error 2
"make -j16 all" terminated with exit code 2. Build might be incomplete.
10:43:15 Build Failed. 2 errors, 0 warnings. (took 626ms)
-------------------
I have cmake 4.0.2 installed. I tried in Ubuntu and Windows, same error.
Can you please help?