Question
STM32CubeMX 6.9.0 released
We are pleased to announce you that the official release of STM32CubeMX V6.9.0 is available for download here
- What is new in STM32CubeMX V6.9.0?
- Added the support for new microcontrollers in the STM32U5 series
- Added the support for new microcontrollers in the STM32WBA series
- Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
- Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
- Added the support for the memory management tool for the STM32H5 and STM32U5 series
- Added the support for new boot paths for the STM32H5 series
- Added makefile generation in dual context for the STM32H7, STM32L5, and STM32U5 series
- Added hierarchical project support in the Example Selector for the STM32U5 and STM32WL series
- Added user authentication functionality
- Added the support for processing before and after code generation
- Upgraded the JDK11 to Adoptium™ Termurin™ 17.0.6
- Main fixed issues
- 121529 [Example selector] Management of hierarchical projects.
- 130926 [Project generation] Makefile project type for dual-context projects is now supported.
- 134482 [Boot path configuration] The boot path functionality now supports the Keil® IDE.
- 144716 [Installer] Added the installation path in the PATH environment variable.
- 145844 [CubeMX][ETH][LwIP] Bug in ethernetif.c file for Nucleo-F429ZI with ETH + LwIP(IPv6)
- 147572 [STM32CubeMX] [SYS] Change in the implementation of stm32l4xx_hal_timebase_tim.c provoked run time issues
- 150288 [MDMA] wrong channel number in the generated code
- 151261 [U5]bug in initialization of GTZC, missing clock enable
- Known issues fixed and problems and limitations
- Please refer to the release note.
- Where do I obtain STM32CubeMX V6.9.0?
- https://www.st.com/en/development-tools/stm32cubemx.html
- … Or update your current installation of STM32CubeIDE using: Help > Check for updates