Skip to main content
Associate
May 5, 2025
Question

STM32CubeMX - Could not create a project for the STM32MP2

  • May 5, 2025
  • 2 replies
  • 615 views

Hello,

I’m unable to create a new project for the STM32MP2 (STM32MP251CAL3) in STM32CubeMX (Version 6.14.1). After selecting the MPU and clicking Start Project, I choose the TrustZone feature—but nothing happens. I can see a “*” appear next to “Untitled” in the top left, but no further dialog appears.

When I try to select an MCU, I receive the warning:

“Project Untitled has been modified would you like to save the projekt?”

If I click Yes, the mouse cursor turns into the blue loading spinner and nothing else happens.

In the Output window, I see:

 Creating: STM32MP251CALx

 Initializing: STM32MP251CALx

 Environment: STM32CubeMX

 

2025-05-05 15_40_18-STM32CubeMX Untitled_.png

 

Even when editing an existing project, I can click options in Pinout & Configuration, but the cursor just shows the blue loading spinner and nothing else occurs.

2025-05-05 15_42_19-STM32CubeMX STM32MP2.ioc__ STM32MP251CALx.png

Could you please help me resolve this?

2 replies

Technical Moderator
May 5, 2025

Hello @pp24 ,

 

First let me thank you for posting and welcome to the ST Community.

I am not able to reproduce the behavior that you described.

I suggest that you provide more details such as the Ioc and the log file.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
pp24Author
Associate
May 5, 2025

Hello @Mahmoud Ben Romdhane ,

 

Thank you for the quick reply.

I can't provide the IOC at the moment, but it's mainly about creating a new one.

 

Regards,

Philipp

Technical Moderator
May 6, 2025

Hello @pp24 ,

I have well received your screen recording and I was not able to reproduce your issue.

The problem is related to your environment. 

I suggest that you delete the cache.

MahmoudBenRomdhane_0-1746539669382.png

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
pp24Author
Associate
June 2, 2025

Hello.

Have you found a solution?

Regards