Skip to main content
JMari.11
Visitor II
July 20, 2023
Question

STM32MP135

  • July 20, 2023
  • 1 reply
  • 1436 views

I would like to Design STM32MP135FA Processor based data logging and file accessing throgh Ethernet 

Kinldy suggest below application possible in STM32MP135 series Processor.

1. Two ethernet going to use - One for SD card file acess / another one for Firmware update / web or ofline GUI in 

2. Linux based system which should be boot from eMMC or NAND flash or DDR3 ( Except SD card)

3. Linux booting should be work in within 6-10 seconds time line.

4. Power back for power shutdown option , so that any PMIC suggest.

5. Internally SQL Database going to store the logging data, so file transfer should be 10MBit /Sec thorugh Ethernet.

6. 2 CAN FD + 4 UART+ SPI+ RTC+USB+ SDRAM  addtional interface and pheriperals.

7. whether Linux boot on this processor avaiable other than SD card Memory?

Please give your suggestion for start the design , also suggest any advance PMIC for avoid the Lunix booting /Runnig file correption.

Waiting for your valuable answer.

Thanks you ... by  Jagathguru Marimuthu

 

1 reply

PNata
Associate
March 18, 2024

We are also looking like this configuration, Could you please share information if you done