Skip to main content
drew
Associate III
July 23, 2020
Solved

STM32MP157 ARM trusted firmware boot error with STM32CubeProgrammer

  • July 23, 2020
  • 3 replies
  • 2934 views

We have a custom board using the STM32MP157C chip and we are having a problem with the USB programming via the CubeMXProgrammer. Our system is working and we have a tf-a.stm32 binary image, a functional u-boot.st32 image and a working rootfs Linux system. We can boot from SDCard and from eMMC.

I have read the flashlayout document which explains the TSV file format and created a layout file for programming the eMMC flash however we are running in to issues actually programming the device via USB.

Here is our TSV file

  #Opt Id Name Type IP Offset Binary

  - 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157c.stm32

  - 0x03 ssbl-boot Binary none 0x0 u-boot.stm32

  PD 0x02 fsbl1 Binary mmc1 boot1 tf-a-stm32mp157c.stm32

  PD 0x04 fsbl2 Binary mmc1 boot2 tf-a-stm32mp157c.stm32

  PD 0x05 ssbl Binary mmc1 0x00100000 u-boot.stm32

  PD 0x10 rootfs System mmc1 0x00300000 rootfs.ext2

The TSV file is parsed correctly by STM32_Programmer_CLI and it downloads the TF-A (ID 0x01) but then hangs.

  Memory Programming ...

  Opening and parsing file: tf-a-stm32mp157c.stm32

   File     : tf-a-stm32mp157c.stm32

   Size     : 245384 Bytes

   Partition ID : 0x01 

  Download in Progress:

  [==================================================] 100% 

  File download complete

  Time elapsed during download operation: 00:00:00.444

  RUNNING Program ... 

   PartID:   :0x01 

We have a serial connection to UART4 to see the boot messages, and when the TF-A starts executing the firmware causes a panic due to the boot interface.

  NOTICE: CPU: STM32MP157C?? Rev.Z

  NOTICE: Model: Custom Board 1 - STM32MP157C

  INFO:  Reset reason (0x14):

  INFO:   Pad Reset from NRST

  INFO:  PMIC version = 0x21

  ERROR:  Boot interface not found

  PANIC at PC : 0x2ffd9b45

  Exception mode=0x00000016 at: 0x2ffd8000

The TF-A source code is the ST branch 2.0 release 3.1: https://github.com/STMicroelectronics/arm-trusted-firmware/releases/tag/v2.0-stm32mp-r3.1

Has anyone seen this error before? Are we missing a configuration option when we build TF-A which would allow for this booting method?

Thank you,

Drew

This topic has been closed for replies.
Best answer by drew

Yes, as stated, we have a functional system, running with TF-A.

The problem was the argument STM32MP_BOOT_ONLY was enabled for the TF-A build, which disables the USB support, this was removed and everything is working.

In plat/st/stm32mp1/platform.mk there are definitions of STM32MP_BOOT_ONLY and STM32MP_FLASHLOADER which appear to be for building smaller more specific versions of TF-A. I expect STM32_FLASHLOADER build argument can be used for building the 'tf-a-serialboot.stm32' as listed (and undocumented) in the flashlayout page https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#e-E2-80-A2MMC

3 replies

Olivier GALLIEN
Technical Moderator
July 24, 2020

Hi @drew​ 

Can you please confirm that you can state "Our system is working " based on flashing eMMC trought SDCard as per describe in your previous post :

https://community.st.com/s/question/0D53W000006Ox3sSAC/stm32mp157-emmc-not-booting

Means that same TF-A is properly booting from eMMC but looks to fail in context of USB flashing.

Thanks

Olivier

Olivier GALLIEN In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
koan
Associate II
July 24, 2020

I strongly suggest you to move all the software components to the latest ST branch 2.2 .

Marco Cavallini - KOAN - https://www.koansoftware.com

drew
drewAuthorBest answer
Associate III
July 29, 2020

Yes, as stated, we have a functional system, running with TF-A.

The problem was the argument STM32MP_BOOT_ONLY was enabled for the TF-A build, which disables the USB support, this was removed and everything is working.

In plat/st/stm32mp1/platform.mk there are definitions of STM32MP_BOOT_ONLY and STM32MP_FLASHLOADER which appear to be for building smaller more specific versions of TF-A. I expect STM32_FLASHLOADER build argument can be used for building the 'tf-a-serialboot.stm32' as listed (and undocumented) in the flashlayout page https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#e-E2-80-A2MMC