STM32MP157C-DK2 disconnects during flashing an is unable to reconnect. Alpha HW?
When trying to flash OpenSTLinux on the STM32MP157C-DK2 the flashing procedure gets halted with the following error message.
16:01:00 : STM32CubeProgrammer API v2.1.0
16:01:01 : USB speed : High Speed (480MBit/s)
16:01:01 : Manuf. ID : STMicroelectronics
16:01:01 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
16:01:01 : SN : 000000000000
16:01:01 : FW version : 0x011a
16:01:01 : Device ID : 0x0500
16:01:19 : Read TSV File: C:\Users\Ludwig\Downloads\en.FLASH-stm32mp1-openstlinux-4.19-thud-mp1-19-02-20\stm32mp1-openstlinux-4.19-thud-mp1-19-02-20\images\stm32mp1\flashlayout_st-image-weston\FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
16:01:19 : Number of partitions: 9
16:01:40 : Start Embedded Flashing service
16:01:40 : Memory Programming ...
16:01:40 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
16:01:40 : File : tf-a-stm32mp157c-dk2-trusted.stm32
16:01:40 : Size : 245360 Bytes
16:01:40 : Partition ID : 0x01
16:01:40 : Download in Progress:
16:01:40 : File download complete
16:01:40 : Time elapsed during download operation: 00:00:00.630
16:01:40 : RUNNING Program ...
16:01:40 : PartID: :0x01
16:01:41 : Start operation done successfully at partition 0x01
16:01:41 : Flashlayout Programming ...
16:01:41 : Running Flashlayout Partition ...
16:01:41 : Flashlayout partition started successfully
16:01:41 : Memory Programming ...
16:01:41 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
16:01:41 : File : u-boot-stm32mp157c-dk2-trusted.stm32
16:01:41 : Size : 748660 Bytes
16:01:41 : Partition ID : 0x03
16:01:41 : Download in Progress:
16:01:42 : File download complete
16:01:42 : Time elapsed during download operation: 00:00:01.138
16:01:42 : RUNNING Program ...
16:01:42 : PartID: :0x03
16:01:42 : reconnecting the device ...
16:02:12 : Error: unable to reconnect the target device: time out expired
16:02:12 : Error: Start operation failed at partition 0x03
16:02:12 : Error: TSV flashing service failed
16:02:12 : Warning: Connection to device 0x500 is lostWhile researching, I stumbled over this particular thread: https://community.st.com/s/question/0D50X0000AgE1buSQC/cant-flash-sd-card-on-stm32mp157xev1-process-stops . This guy had a similar problem as I do. My MB1272 is also green instead of blue like on all the images I saw. This device was provided to me as a part of an urgent project, but I can't seem to get it working. Please provide a solution for me, so I can start working. Thanks to anyone in advance!