undefined reference to `HAL_NVIC_SetPriority'
Hello,
I create new STM32 project for STM32MP131AAG3 with baremetal.
I encounter the following errors when to build the codes of DMA generated by STM32CubeMX.
- undefined reference to `HAL_NVIC_SetPriority'
- undefined reference to `HAL_NVIC_EnableIRQ'
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX1_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream1_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
}
I fixed the code as follows.
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMAMUX1_CLK_ENABLE();
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA interrupt init */
/* DMA2_Stream1_IRQn interrupt configuration */
IRQ_SetPriority(DMA2_Stream1_IRQn, 0);
IRQ_Enable(DMA2_Stream1_IRQn);
}
Is this bug? Or is there possibility that I took mistake MX settings or else?
If it is bug, is there a plan to apply this bug fix to the STM32CubeMP13 codebase?
I am in trouble since the code reverts when I change MX settings.