Question
When I try to program STM32MP157A-DK1 it says No ST-LINK detected. I tried to install 1.8.0 in Linux but it installed Version: 1.7.0 Build: 10852_20210715_0634 (UTC) instead.
The Nucleo F446RE pops up with a media directory as soon as I plug the USB into the ST-Link
The STM32MP157A-DK1 does not do that. And when I try to program it it says NO ST-LINK Detected.
I have tried the Boot switches in every position but I understand Boot 0 Off, and Boot 2 On should let me program the M4 over the ST-Link.
Help.