Question
Yocto STM32MP157 DK2 - Display not working
Hello
I use https://github.com/STMicroelectronics/meta-st-stm32mp with the stm32mp15-disco machine.
It boots fine, I can access the shell via USB-UART. But the display just shows an STM Logo from the Bootloader. What do I need to change, so the display works in Linux?
This is the error when trying to start X:
root@stm32mp15-disco:~# startx
xauth: file /home/root/.serverauth.724 does not exist
X.Org X Server 1.21.1.8
X Protocol Version 11, Revision 0
Current Operating System: Linux stm32mp15-disco 6.1.28 #1 SMP PREEMPT Thu May 11 14:04:52 UTC 2023 armv7l
Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
Current version of pixman: 0.42.2
Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.0.log", Time: Fri Mar 9 21:17:20 2018
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
(EE)
Fatal server error:
(EE) no screens found(EE)
(EE)
Please consult the The X.Org Foundation support
at http://wiki.x.org
for help.
(EE) Please also check the log file at "/var/log/Xorg.0.log" for additional information.
(EE)
(EE) Server terminated with error (1). Closing log file.
xinit: giving up
xinit: unable to connect to X server: Connection refused
xinit: server error