Skip to main content
Amelie ACKERMANN
Community Manager
February 19, 2025

Latest STM32C0 MCUs ease entry into embedded development

  • February 19, 2025
  • 2 replies
  • 3778 views

Three new microcontrollers (MCUs) are joining the STM32C0 series, giving designers more flexibility with options including greater memory density, extended interfaces, and CAN FD for enhanced communication capability.

The new MCUs now joining the cost-efficient series include the STM32C051, with up to 64 KByte of flash for applications that need more storage than STM32C031 MCUs can provide. Additional features include extra interfaces and more user I/O channels in packages with up to 48 pins.

Also new, the STM32C091 and STM32C092 extend flash density up to 256 KByte in packages up to 64 pins, adding a CAN FD interface in the STM32C092. With CAN FD on-chip, users can trim the BOM and simplify the hardware design of industrial communication and networking devices, leveraging the upgraded protocol’s flexibility, speed, and payload capacity.

obn-stm32c0-series-ss2200.jpg

 

"The STM32C0 series offers great flexibility as a cost-conscious line in the STM32 family, with memory ranging from 32 KByte to 256 KByte of flash and rich peripherals," commented Patrick Aidoune, General Purpose MCU Division General Manager, STMicroelectronics. "The large flash and RAM now available in the STM32C091/C092 let designers host the graphical user interface alongside the main application, leveraging ST’s TouchGFX tools to create entertaining experiences and streamline development."

As the most affordable entry point to the STM32 family, STM32C0 MCUs contain widely used interfaces such as crystal-less USB Full Speed Device and USARTs, as well as timers and an analog/digital; converter (ADC). Complementing the cost-conscious feature set, the economical design with on-chip clocks and just one power-supply input saves additional external components including timing and decoupling from the bill of materials (BOM). Further, these savings enable a smaller, simpler PCB design.
7426023_Nucleo-C092RC-top view.jpg6628421_estore_NUCLEO-C051C8-recto.jpgAll STM32C0 MCUs come with extra benefits for developers, including ST’s extended longevity program that ensures long-term availability throughout the lifetime of industrial projects. As members of the high-quality STM32 family, designing with STM32C0 MCUs also eases compliance with product-level approvals such as IEC 61508 for functional safety. The devices contain the Arm® Cortex®-M0+ core that also powers STM32G0 MCUs, which are designed for higher performance and advanced features. The two STM32 MCU series share many aspects including package styles and pinout, and peripheral IP, enabling designs to migrate easily between the two.

The latest STM32C0 microcontrollers are in production now, priced from $0.426 for STM32C051F8P6, $0.682 for the STM32C091FCP6, and $0.733 for the STM32C092FCP6 with CAN FD, for orders of 10,000 pieces.

STM32C0-boards-for-devnews.jpg

Additional resources

First published on Feb 19, 2025

2 replies

Simon.T
ST Employee
February 19, 2025

We are excited to announce the launch of our new product lines. If you have any questions or comments, please feel free to share them here.

We hope you will enjoy the three new STM32C0 MCUs, especially the STM32C092 devices and the new NUCLEO-C092RC board with embedded FD-CAN PHY.

Visitor II
May 19, 2025

I have a very space-constrained application with FDCAN, so I'm curious when the STM32C092EC (WLCSP24 package) will be available