Skip to main content
Associate
July 25, 2025
Question

Can't build on VSCode

  • July 25, 2025
  • 2 replies
  • 685 views

Hello, I have opened someone else's STM32 project in VSCode but I'm getting errors and I can't build. I think it has something to do with CMake, the extension is not asking me to generate a CMAKE config. Do I have to genereate a new project from IDE/MX to work with CMAKE or can I generate the CMAKE files in the exisiting project?

 

Also, it seems that the extension wants you to disable clangd or cpp intellisense extensions because they conflict with the extension's intellisense, is there a way to enable the extention intellisense only for STM32 projects?

Thanks in advance

hasansyr_0-1753450249011.png

 

2 replies

Cartu38 OpenDev
Graduate II
July 25, 2025

If you prefer Microsoft C/C++ extension code indexing just disable or unsinstall STM32Cube one

Cartu38OpenDev_0-1753454672090.png

STM32Cube is adding indexing directives for both conributors Microsoft & clangd ... so you have choice !

hasansyrAuthor
Associate
July 26, 2025

I know I can disable the extensions, my question was if I can use the STM32 one only for STM32 projects since it seems best.

ST Employee
July 28, 2025

@Cartu38 OpenDev is right, currently - but more ambition here in future, so rational for forking today - promoted STM32Cube clangd extension is on par vanilla one except STM32Cube bundles management addition serving you clangd utility another way.

This extension can be disabled, we are promoting settings for both clangd and Microsoft C/C++ extension embedded indexer, allowing end user to get choice.

VSCode is not supporting to enable / disable an extension per project but workspace based it's possible if helping:

vincent_grenet_0-1753684165900.png

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Cartu38 OpenDev
Graduate II
July 25, 2025

"someone else's STM32 project in VSCode" processed Thanks STM32Cube already (sign of is / do you get at project root a .settings\ide.store.json) ? 

Cartu38 OpenDev
Graduate II
July 25, 2025

Any trace / log / snapshot more to share about build issue ?

hasansyrAuthor
Associate
July 26, 2025

There is no build error because I didn't build, there is no build icon maybe because of the missing CMAKE config