Skip to main content
Associate II
January 7, 2026
Solved

Cannot find nucleo board in VSCode Page Setup

  • January 7, 2026
  • 1 reply
  • 498 views

Hello,

 

I am trying to set up a project using STM32Cube Extension in VS Code. When I attempt to select the Nucleo‑F207ZG board in the Board/Device selector, the board does not appear in the list.

modecs_0-1767764804313.png

The stm32cube_core output shows the CMSIS_PACK_ROOT environment variable, and under that directory the file .Download\cache\scanner_391867825626163.cache contains entries for nucleo-f207zg as well as STMicroelectronics.nucleo-f207zg_hw-board.1.0.0.pdsc. Despite these files being present, the board is still not discovered by the IDE.

 

Could you please advise what additional checks or steps I should perform to resolve this issue?

1 reply

ST Employee
January 7, 2026

@modecs 
Nucleo‑F207ZG board is supported. Please provide more details in the search text field to clarify your request. The drop-down list is intentionally limited in item count because the STM32 portfolio includes more than 4000 devices.

vincent_grenet_0-1767767341182.png

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
modecsAuthor
Associate II
January 7, 2026

I am aware of that as well. As described above, when using STM32Cube → STM32CUBE KEY ACTIONS → Setup STM32Cube project(s) and searching for Nucleo‑F207 in the Board/Device dialog, the board does not appear, as shown in the screenshot.

modecs_0-1767769584438.png

I suspect that the extension fails to retrieve the board/device information, causing the entries for this board and its associated IC to be omitted. The missing entries include all Nucleo boards that use the F2 and F4 series, as well as the entire STM32F2 and STM32F4 IC families.

vincent_grenetBest answer
ST Employee
January 7, 2026
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.