Skip to main content
AHugh.2
Associate III
August 6, 2025
Solved

Identifying updatable items in the bundles manager

  • August 6, 2025
  • 3 replies
  • 555 views

Hi,

In the bundles manager for my project is it possible to view at a glance items where there is an update available? Currently the status column icon doesn't differentiate between updatable items - only when I open the version drop-down does it become clear there are newer version(s) available (or I select all then hover over the update button).

Also, same goes for "cube pack list" command - can this show a list of updatable items?

Thanks.

Best answer by vincent_grenet

@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.

3 replies

Cartu38 OpenDev
Graduate II
August 7, 2025

Status column is right one and sortable. Variation is thin but exists. Check icon is not exactly same. One is negative of the second. Looks at it carefully.

Way to update them all thanks VSCode integrated terminal is 'cube bundle update'

I've not found way to list updatable for packs. Here way to sync. is 'cube pack sync'

AHugh.2
AHugh.2Author
Associate III
August 7, 2025

If you look at the "System" bundles manager then yes, there is a difference in the icon, but in the project one there is not.

AHugh2_1-1754551877081.png

So here, 1.0.0 is bold and selected indicating it is the current one, but there is a newer 1.0.1 one, but the icon in the status column is indentical as far as I see.

Very minor point!

vincent_grenetBest answer
ST Employee
August 7, 2025

@AHugh.2 Thanks for reporting. I acknowledge this minor issue and I can share already this is fixed in our current code base. Will be part of next update planned already in coming weeks.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Employee
August 18, 2025

Please be aware that stm32cube-ide-bundles-manager-0.23.3.vsix has been released to address reported concerns.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.