Issue with "multilib.yaml" error when using ST_ARM_CLANG in VS Code
Hi,
I am using the latest version of STM32Cube extension for VS Code (3.8.0). I created a simple project for STM32H735G-DK board using CMake as the toolchain and ST-ARM-CLANG as the compiler. I do not know if it is relevant, but I also enabled FreeRTOS and configured the USE_NEWLIB_REENTRANT option to Enabled.
I generated the project and I am compiling it with VSCode. I changed in the starm-clang.make to use the NEWLIB instead of the PICOLIBC:
set(STARM_TOOLCHAIN_CONFIG "STARM_NEWLIB")The compilation works, but clangd complains about some errors. In the output of clangd, I can see multiple instances of:
D:\ST\stm32cube\bundles\st-arm-clang\21.1.1+st.6\bin\..\lib\clang-runtimes\multilib.yaml:47:3: error: unknown key 'IncludeDirs'
IncludeDirs:
^~~~~~~~~~~
D:\ST\stm32cube\bundles\st-arm-clang\21.1.1+st.6\bin\..\lib\clang-runtimes\multilib.yaml:21:1: error: multilib "arm-none-eabi/armv4t_exn_rtti_size" specifies undefined group name "stdlibs"
MultilibVersion: '1.0'
^and because of these errors some headers are not found, like:

Thank you!