Skip to main content
Visitor II
September 9, 2025
Solved

L6218E: Undefined symbol errors with armlink on STM32G474x

  • September 9, 2025
  • 1 reply
  • 1056 views

MCU: STM32G474xx
IDE: VSCode
Toolchain: ARM Compiler 6 (armclang, armlink)
Question:

I'm a newcomer to using armclang and armlink for compiling and linking a project for an STM32G4 MCU. I've successfully compiled a minimal project and am trying to link it using armlink.

My scatter file is:

LR_IROM1 0x08000000 0x00080000 { ; load region size_region
 ER_IROM1 0x08000000 0x00080000 { ; load address = execution address
 *.o (.isr_vector, +First)
 *(InRoot$$Sections)
 .ANY (+RO)
 .ANY (+XO)
 }
 RW_IRAM1 0x20000000 0x00020000 { ; RW data
 .ANY (+RW +ZI)
 }
}

I use a startup script in GNU syntax generated from CubeMX.
The linker command I am using is: armlink --cpu=Cortex-M4.fp.sp *.o --scatter=STM32G474XX_FLASH.sct --map --info=summarysizes --load_addr_map_info --xref --callgraph --symbols --info=sizes --info=totals --info=unused --info=veneers

This setup results in the following linking errors:

Error: L6218E: Undefined symbol _sidata (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol _sdata (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol _edata (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol _sbss (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol _ebss (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol __libc_init_array (referred from startup_stm32g474xx.o).
Error: L6218E: Undefined symbol _estack (referred from startup_stm32g474xx.o).

I understand that the scatter file defines memory regions, but it seems I also need to define these specific symbols (_sidata, _sdata, _estack, etc.) for the linker. How do I properly define these symbols within the .sct file, and what is the correct way to resolve the missing __libc_init_array function?

Best answer by mƎALLEm

Hello @amoehring99 and welcome to the community,

It seems like your project is pointing to a wrong startup file from GCC (Drivers\CMSIS\Device\ST\STM32G4xx\Source\Templates\gcc\startup_stm32g474xx.s)

_sidata, _sdata etc.. are located in the .s file of GCC.
You need to link the .s file of arm.

Try to link the file Drivers\CMSIS\Device\ST\STM32G4xx\Source\Templates\arm\startup_stm32g474xx.s to your project instead what you have.

 

1 reply

mƎALLEm
mƎALLEmBest answer
Technical Moderator
September 18, 2025

Hello @amoehring99 and welcome to the community,

It seems like your project is pointing to a wrong startup file from GCC (Drivers\CMSIS\Device\ST\STM32G4xx\Source\Templates\gcc\startup_stm32g474xx.s)

_sidata, _sdata etc.. are located in the .s file of GCC.
You need to link the .s file of arm.

Try to link the file Drivers\CMSIS\Device\ST\STM32G4xx\Source\Templates\arm\startup_stm32g474xx.s to your project instead what you have.

 

"To give better visibility on the answered topics, please click on ""Accept as Solution"" on the reply which solved your issue or answered your question."