Linking DPC_AverageCurrentCtrl_IAR.a with VS Code and CMake?
Hi everyone,
I'm working on a power conversion project using the STEVAL-7BIDIRCB reference design.
The firmware uses a specific static library: DPC_AverageCurrentCtrl_IAR.a. As the name suggests, it was compiled with IAR EWARM. However, I would like to use VS Code and CMake for my development environment instead of the IAR IDE.
A few questions:
Is this specific library compatible with the arm-none-eabi-gcc linker in a CMake setup, or will I face ABI/runtime issues (especially regarding FPU and math functions)?
If I use the IAR Build Tools (compiler/linker) through CMake in VS Code, will it work seamlessly with this .a file?
Is there a GCC version of this library available for the STEVAL-7BIDIRCB, or are the sources available somewhere to recompile it for GCC?
The control loop is obviously critical for this board, so I want to make sure I don't introduce any instability by mixing toolchains.
Thanks for your help!