Reprogram when MCU is in stop mode.
Hello! I am using an STM32U545 and VS Code for programming. I am experiencing the following issue: I am working with STOP mode, and once the MCU enters this state, I can no longer reprogram it. When using STM32CubeIDE, I did not encounter this problem (I believe this is related to the connect-under-reset feature, which VS Code seems to lack when programming).
Is there anything I can do to avoid this issue, other than using STM32CubeProgrammer to erase the memory or adding a delay at the start of the program to give myself time to program the device after a manual reset?