STM32H563 Application boots only with manual linker/VTOR edits, fails when generated via CMake:
- February 4, 2026
- 2 replies
- 358 views
I am working on an STM32H563 project with a custom bootloader and two application slots (APP1 / APP2).
This is my memory layout
- Bootloader: 0x08000000
- APP1: 0x08022000
- APP2: 0x0806C000
The bootloader is already deployed in the field and cannot be modified.
The bootloader jump sequence is standard:
- Validate application
- Set SCB->VTOR = APPx_START_ADDRESS
- Load MSP from APPx_START_ADDRESS
- Jump to reset handler at APPx_START_ADDRESS + 4
This works perfectly when I build the application the “manual” way:
- Manually change FLASH ORIGIN in the application linker script to 0x08022000
- Manually change VECT_TAB_OFFSET in system_stm32h5xx.c
- Then i ReBuild → flash → bootloader jumps and application runs correctly.
I would like to automate this process using cmake , without manually editing the linker script and system_stm32h5xx.c
So I implemented:
- A parameterized linker script template (STM32H563xx_FLASH.ld.in)
- CMake configure_file() to generate slot-specific linker scripts
- CMake target_compile_definitions() to inject VECT_TAB_OFFSET
target_compile_definitions(app1 PRIVATE
VECT_TAB_OFFSET=0x00022000
)In the linker template .ld.in file, i have this:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 640K
FLASH (rx) : ORIGIN = @FLASH_ORIGIN@, LENGTH = @FLASH_LENGTH@
}FLASH_ORIGN and FLASH_LENGTH are the variables
The generated .ld correctly shows FLASH (rx) : ORIGIN = 0x08022000, and i checked using STM32 cube programmer that the hex file is programmed at the correct address.
The problem is that when i generate the hex files from cmake , once i flash them in , the bootloader does not jump to the application.
Am i missing any obvious step here? I have attached the cmakelist file and the linker template(STM32H563xx_FLASH.ld.in)
Kindly Help