Support for TrustZone and MultiCore
Quick question.
I am working on two projects:
- One is a dual-core project, and uses the STM32H755 and CMSIS-RTOS v2 over Free RTOS.
- I often have to debug two boards simultaneously.
- I often have to debug two boards simultaneously.
- Another project is using STM32H573. This uses TrustZone and ThreadX (on the non-secure side).
Both are currently managed via ST Cube IDE (Eclipse based of course) and debugging is already quite "complex".
I can see advantages with VS Code, but moreover, I would not be surprised if the VS Code route becomes the de-facto standard some day (purely speculative of course), so I think I may need to start looking at it.
Before I do, my question to the community is whether the VS Code option is yet mature enough for dual core and TrustZone projects?
Many thanks in advance,
Nick